Overview: Database Table

Use this operation to import a dataset by connecting to a OLE DB or ODBC provider data source and selecting the database where the tables are listed. You can select to either generate a query which will enable you to import all the fields and rows selected, or you can enter your own query, allowing control over what columns and/or rows are imported.

NOTE: CSense provides secure native blocks and operations for building analytics and solutions. The native capabilities provided by CSense can be extended by making use of this feature. When making use of this feature, please ensure that you have validated your extended functions to ensure that they perform as intended and do not introduce stability or security risks to your production system. Do not use scripts or components from untrusted sources.

Properties

Category:

Import

Performance risk:

Potential high performance risk. The performance is influenced by the size of the text file being imported, which is determined by number of rows and/or the number of columns of the dataset.

Knowledge required:

None

 

Effect on datasets

How many datasets are required to perform this operation?

N/A

Does it create a new dataset?

Yes

Can you reconfigure this operation?

Yes

Can you apply this operation to a locked dataset?

N/A

Does it modify the current dataset in any way?

N/A

Requirements

  • Connection to a data source and configuring the following security permissions:

    • Server name: the name of the SQL server

    • Access file: the name of the file where the Access database is saved.

    • Login: select to use either Windows authentication or server authentication, which will prompt you to enter a username and password

    • Database: select one of the listed databases from the drop down menu.

    When you read data from a table that contains a DATETIME2 field, you must use the “SQL Server Native Client” OLE DB provider for it to be recognized as a timestamp field. The “Microsoft OLE DB Provider for SQL Server” and “… for ODBC Drivers” will not work (not support by Microsoft) and will recognize DATETIME2 as a string.

Results

  • The table from the selected database will be imported as a dataset. The columns will depend on the selected SQL query used to import the fields and rows.


Related topics:

  

CSense 2023- Last updated: June 24,2025